T2080 Linux.uImage binary

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 Linux.uImage binary

1,169件の閲覧回数
clay_s_brice
Contributor I

How can I get a Linux.uImage for a T2080qds system? The image resides at flash address E8020000 and EC020000 and is approximately 7 MB. The flash there was inadvertently erased. If I can get a binary image that I can re-load that would be great. Thanks

0 件の賞賛
返信
1 返信

1,073件の閲覧回数
ufedor
NXP Employee
NXP Employee

Pre-built images (including uImage) are provided on the QorIQ Linux SDK v2.0 PPC64E6500 IMAGE.iso and QorIQ Linux SDK v2.0 PPCE6500 IMAGE.iso which can be downloaded from:

Linux® SDK for QorIQ® Processors | NXP 

Also the ISOs contain complete NOR Flash images.

0 件の賞賛
返信