T2080 Hardcoded RCW inconsistencies

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T2080 Hardcoded RCW inconsistencies

跳至解决方案
2,669 次查看
benjaminlux
Contributor I

Inconsistencies found on [1] : QorIQ T2080 Family Reference Manual, Rev. 1 05/2015.

Could you help clarify the correct values for cfg_rcw_src please ?

  1. pp197, 198 of [1], we can see that cfg_rcw_src[0]_[1:4]_[5:8] values for booting from Hard coded RCW should be 0_1001_1010, 0_1001_1100, or 0_1001_1110 i.e. 0x9a, 0x9c or 0x9e. Where aspp 216, the table 4-15 of clock frequencies for the hardcoded options present the following values for cfg_rcw_src[0]_[1:4]_[5:8] : 0_1000_1100, and 0_1000_1111 i.e. 0x8c and 0x8f. Shouldn’t these values be the same?
  2. The table 4-15, presents the same frequency values for the 2 values of the cfg_rcw_src value. Shouldn’t they be different? Would you be able to provide us with the frequency configurations that will actually be available ?
  3. On the top right corner of the table 4-16 pp. 216-217 values for hardcoded options are 0x86, 0x87. Again, this looks incompatible with the previously presented values.
标签 (1)
0 项奖励
回复
1 解答
2,317 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Now the manual Rev. 2, 02/2016 is available on the NXP site. Table 4-15 and Table 4-16 have been corrected. Now Table 4-15 and Table 4-16 show Hard Coded RCW Options as 0_1001_110x and 0_1001_111x . Also both these tables now show that SysClk is different for these 2 options (66.7 and 133 MHz).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,318 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Now the manual Rev. 2, 02/2016 is available on the NXP site. Table 4-15 and Table 4-16 have been corrected. Now Table 4-15 and Table 4-16 show Hard Coded RCW Options as 0_1001_110x and 0_1001_111x . Also both these tables now show that SysClk is different for these 2 options (66.7 and 133 MHz).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,317 次查看
benjaminlux
Contributor I

Thank you very much Serguei for this fresh update.

Regards,

0 项奖励
回复