T2080 HARDCODED RCW INCONSISTENCY W.R.T TOOL AND RM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 HARDCODED RCW INCONSISTENCY W.R.T TOOL AND RM

2,263 Views
tkchaitanya
Contributor II

Hi,

Also kindly confirm that as per the tool there are 2 two combinations for RCWs

1. with 0x8C Sys_Clk=66.7MHz,DDR_Clk=133.33MHz

2. with 0x8F Sys_Clk=66.7MHz,DDR_Clk=133.33MHz

What is the difference on above both and can I use the following combination

Sys_Clk=133.33MHz and DDRClk=66.7MHz

Kindly help on above.

0 Kudos
Reply
3 Replies

2,255 Views
ufedor
NXP Employee
NXP Employee

> per the tool

Which tool?

0 Kudos
Reply

2,243 Views
monalihaware
Contributor III

As per pbl utility in the qcvs tool.

0 Kudos
Reply

2,230 Views
ufedor
NXP Employee
NXP Employee

Description in the T2080 RM is correct.

QCVS has to be fixed.

0 Kudos
Reply