T2080 HARDCODED RCW INCONSISTENCY W.R.T TOOL AND RM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 HARDCODED RCW INCONSISTENCY W.R.T TOOL AND RM

2,279件の閲覧回数
tkchaitanya
Contributor II

Hi,

Also kindly confirm that as per the tool there are 2 two combinations for RCWs

1. with 0x8C Sys_Clk=66.7MHz,DDR_Clk=133.33MHz

2. with 0x8F Sys_Clk=66.7MHz,DDR_Clk=133.33MHz

What is the difference on above both and can I use the following combination

Sys_Clk=133.33MHz and DDRClk=66.7MHz

Kindly help on above.

0 件の賞賛
返信
3 返答(返信)

2,271件の閲覧回数
ufedor
NXP Employee
NXP Employee

> per the tool

Which tool?

0 件の賞賛
返信

2,259件の閲覧回数
monalihaware
Contributor III

As per pbl utility in the qcvs tool.

0 件の賞賛
返信

2,246件の閲覧回数
ufedor
NXP Employee
NXP Employee

Description in the T2080 RM is correct.

QCVS has to be fixed.

0 件の賞賛
返信