T2080 Descriptor Command fields

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 Descriptor Command fields

1,436件の閲覧回数
Faizanbaig
Contributor IV

Hi ,

I am trying to develop Crypto driver for T2080. I have a doubt related to the descriptor command fields .

The macros available in desc.h file of SDK seems to set Command bits following bit positions 31,30,29,28.....2,1,0(MSB-LSB) but for example FIFO LOAD Command Format in the T2080 SEC Reference Manual has the bit positions as 0,1,2.........28,29,30,31(LSB-MSB).

So do we need to use the macros availabe in desc.h as is or do we need to change the macros setting as per T2080SECRM bit ordering?

Any help would be appreciated.

 

Thanks,

Faizanbaig Inamdar

 

 

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)