T2080 Descriptor Command Fields

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 Descriptor Command Fields

1,973件の閲覧回数
chitra_amzarewa
Contributor II

Hello,

I am developing Crypto driver for T2080. Descriptor command fields seem to be confusing.

The macros available in desc.h file of SDK seems to set Command bits following bit positions 31,30,29,28.....2,1,0(MSB-LSB) but for example FIFO LOAD Command Format in the T2080 SEC Reference Manual has the bit positions as 0,1,2.........28,29,30,31(LSB-MSB).

Both fields are contradicting, can you provide additional information if macros in desc.h should be used as is or macros need changes as per T2080SECRM bit ordering?

Any help would be appreciated.

Thanks & Regards,

Chitra Amzarewale

@Faizanbaig 

ラベル(1)
0 件の賞賛
返信
1 返信

1,954件の閲覧回数
Faizanbaig
Contributor IV

Could somebody please help us in this?

0 件の賞賛
返信