T1042D4RDB SerDes Memory Mapping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042D4RDB SerDes Memory Mapping

2,627 Views
burakorcun_ozka
Contributor III

Hello,

I'm working with u-boot on T1042D4RDB, and have some question about SerDes memory mapping.

  1. Is there a maximum physical memory region which is allocated by CPU for SerDes ? If so, is there any documentation about CPU physical memory mapping limits?
  2. If SerDes has a maximum physical memory region, can i set custom size TLBs and LAWs inside this memory region? For example, according to 0x06 SerDes configuration, SerDes has 4 PCIe buses. Can these buses have custom-size memory regions? Is there any constraint about minimum size or maximum size for each bus?
  3. Does maximum SerDes memory region depend on CPU or board? I mean, is it configurable size from board to board?

Thanks in advanced.

0 Kudos
Reply
4 Replies

2,563 Views
ufedor
NXP Employee
NXP Employee

Posed questions can't be answered because no "physical memory region is allocated by CPU for SerDes".

Please read QorIQ T1040 Reference Manual, Chapter 2 Memory Map

0 Kudos
Reply

2,563 Views
burakorcun_ozka
Contributor III

ufedor,

I'm a little confused and, just wonder that how u-boot know the following addresses for PCIe busses.

0xF_FFDF_0000 0xF_FFDF_0FFF IFC - CPLD 4KB
0xF_FF80_0000 0xF_FF80_FFFF IFC - NAND Flash 64KB
0xF_FE00_0000 0xF_FEFF_FFFF CCSRBAR 16MB
0xF_F803_0000 0xF_F803_FFFF PCI Express 4 I/O Space 64KB
0xF_F802_0000 0xF_F802_FFFF PCI Express 3 I/O Space 64KB
0xF_F801_0000 0xF_F801_FFFF PCI Express 2 I/O Space 64KB
0xF_F800_0000 0xF_F800_FFFF PCI Express 1 I/O Space 64KB
0xF_F600_0000 0xF_F7FF_FFFF Queue manager software portal 32MB
0xF_F400_0000 0xF_F5FF_FFFF Buffer manager software portal 32MB
0xF_E800_0000 0xF_EFFF_FFFF IFC - NOR Flash 128MB
0xF_0000_0000 0xF_003F_FFFF DCSR 4MB
0xC_3000_0000 0xC_3FFF_FFFF PCI Express 4 Mem Space 256MB
0xC_2000_0000 0xC_2FFF_FFFF PCI Express 3 Mem Space 256MB
0xC_1000_0000 0xC_1FFF_FFFF PCI Express 2 Mem Space 256MB
0xC_0000_0000 0xC_0FFF_FFFF PCI Express 1 Mem Space 256MB
0x0_0000_0000 0x0_ffff_ffff DDR 2GB

These busses are on SerDes lanes, and mem spaces have 256 MB physical memory range.

Can i use an address that is out of 0xC_3FFF_FFFF or 0xC_0000_0000 for a PCIe device? Is 0xC_0000_0000 a start address for busses on SerDes?

Additionally, i didn't see anything about SerDes in Memory Chapter. If there is, could you please tell me a chapter number?

0 Kudos
Reply

2,563 Views
ufedor
NXP Employee
NXP Employee

Please read the QorIQ T1040 Reference Manual, Chapter 28 PCI Express Interface Controller.

You wrote:

> the following addresses for PCIe busses

How these data was obtained in U-Boot?

0 Kudos
Reply

2,563 Views
burakorcun_ozka
Contributor III

ufedor,

Are these physical addresses that u-boot uses completely arbitrary? Can i use 0xA_0000_0000 - 0xA_0FFF_FFFF instead of 0xC_0000_0000 - 0xC_0FFF_FFFF for any PCIe device?

I think, statement of SerDes address that starts from 0xC_0000_0000, as i said, is not correct. I mistook.

But, there is still fixed address block in T1042 like boot window only. Is it true?

0 Kudos
Reply