T1042 DIU interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 DIU interface

1,359 Views
ilhanbey
Contributor I

Dear Responsible;

In T1042RDB For LVDS interface the used transmitter DS90C387R is -10~+70C rated and i need an extended counterpart with at least -40~+85. could you pls recommend me an alternative?

I found

DS90C385A
DS90C383B
SN65LVDS93B-Q1
(DS90CR287)
(DS90CR285)
THC63LVDM83D-Z
THC63LVDM83C(5S)
THC63LVDM83D

as alternatives but not sure one of them is okey. 

DS90C387R has 12 bit data interface but the above alternatives have 24-bit data?

By the way, is there any tutorial about DIU explaining it deeply?

Regards

0 Kudos
Reply
1 Reply

1,308 Views
Pavel
NXP Employee
NXP Employee

The 1042 DIU supports double-pumped pixel data for a low-pin count, 12-bit-wide DDR pin interface to support up to 24-bit RGB.

Find LVDS double transmitter.

See the VT1631:

https://www.viatech.com/en/silicon/legacy/video-display/vt1631/https://www.viatech.com/en/silicon/legacy/video-display/vt1631/

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply