T1040d4 custom board without CPLD, JTAG programming issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1040d4 custom board without CPLD, JTAG programming issue

跳至解决方案
2,118 次查看
Wj_khi
Contributor II
Hi I have custom board designed using T1040d4 qoriq powerpc. My bareboard powerpc is currently power on using onboard power sequencing without using any CPLD. Right now i have no serial interface to monitor and debug it as both T1040 UART interfaced are attached with some other hardware over custom board. #Issue# when attached via CW usb tap its Jtag unable to program and flash bootloader via code warrior it shows " IR scan measure error" also "core not responding " in jtag log console.
0 项奖励
回复
1 解答
1 回复