T1040 Voltage Ramp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1040 Voltage Ramp

1,271件の閲覧回数
darrellblock
NXP Employee
NXP Employee

Customer has T1040 power-up question.  They are planning on having all voltage rails come up ratiometrically (see image).  This looks to be OK but they would like verification.


T1040 Voltage Ramp.png
   
 
 
 
 
 
 
 
 
 
 
 





ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,175件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1040 data sheet available on the NXP site (link) provides  the power sequencing requirements. It should be satisfied. There are 3 groups of power supplies. There is not ordering requirement with respect to one another in the same group. Groups 1,2 and 3 must be ordered sequentially such that voltage rails on a previous step must reach 90% of their value before the voltage rails on the current step reach 10% of theirs

Ramp-up.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信