T1040 DIU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040 DIU

1,433 Views
muhammadyasirqa
Contributor I

Dear All

I am designing a custom board around T1042 Processor. I want to interface the T1042 with a VGA Display. I have spotted a DIU interface but it is quite different from the traditional one in MPC5125 where a parallel interface of 8x3 bits is available. I cannot find a COTS IC for interfacing this type of DIU of T1042 to VGA. Could you please suggest one? Regards

Yasir

Labels (1)
0 Kudos
Reply
1 Reply

1,283 Views
ufedor
NXP Employee
NXP Employee
The following devices were tested with the T1042 DIU:
CH7301C for HDMI
DS90C387R for LCD
TFP410PAP for DVI