T1040 DDR3 ECC Strategy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1040 DDR3 ECC Strategy

1,025件の閲覧回数
adamgarrison
Contributor III

I am using a 72b DDR3 interface on the T1040.  Using the 72 bit interface normally locks me into using x8 ICs because it only has 8 bits of ECC. What I’m curious about though, would be the possibility of using x16 chips to save space. I could see two possibilities, and I’m just not enough of an expert on SDRAM to know if this would work or just cause more problems than it’s worth. I  would either propose:

   -Use Qty 5 x16 ICs, leaving the upper 8 data bits of the ECC IC unconnected or grounded.

   -Use Qty 4 x16 ICs, and Qty 1 x8 IC for ECC

 

I’m wondering if either of these schemes would work, and if so, which would be preferred?

 Thank you,

Adam

ラベル(1)
0 件の賞賛
返信
1 返信

930件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

For sure you can use 5 x16 ICs, leaving the upper 8 data bits of the ECC IC unconnected or terminated. Typically unused DQ can be left unconnected while control input like DM should be terminated. You can ask DRAM producer for details. This case is preferred.

You may also use 4 x16 ICs, and 1 x8 IC for ECC if SDRAM organisation and timing of the 16 IS and 8 IS are the same.

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信