T2080QDS not booting U-Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080QDS not booting U-Boot

1,287 次查看
eliezerfernande
Contributor I

The T2080QDS is not booting anymore. U-Boot doesn't show up on the serial connection. I'm using a dummy terminal to connect to the board using 115200 as the baud rate. We have another T2080QDS board that actually boots up, so it is that specific board giving us trouble. The board used to connect previously so we're not sure what happened. We were trying to make it boot from a SD card (with the same process as the other one, and the other one works) so we are afraid that has messed something up. Is there a way to make the board boot U-Boot again? Thanks!

标签 (1)
0 项奖励
回复
1 回复

1,025 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Eliezer Fernandez ,

1. Please compare switch settings between these two boards.

2. Please download image ISO for e6500 from Linux® SDK for QorIQ Processors|NXP, get SD u-boot image to copy it in the first partition of a SD card. Plugin SD card to the target board and configure the target boot from SD.

3. Do you have CodeWarrior TAP? If so, please download CodeWarrior 10.5 to debug the target board to find the exact problem.

Thanks,

Yiping

0 项奖励
回复