T1024 evaluation boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 evaluation boards

1,599件の閲覧回数
EAlepins
Contributor V

Hi,

We are seeking to buy a T1024 evaluation board. I searched the Internet, but found a very few options:

- NXP T1024RDB: has DDR3L memory

- MicroSys miriac SBC-T1024: DDR4 memory, non standard JTAG connector (JST BM14B-SrSS-TB 14 pins connector or a Tag-Connect TC2050-IDC-FP 10 pins connector; rather than standard 16 pins)

That's all. We have not decided yet which type of DDR we'd want, but we like to have more options. We have no certification requirement for the board since it will only be used for initial code development before we receive our custom board. Are you aware of other vendors, especially for DDR4 option?

Thanks.

Étienne

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,479件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is only one T1024-based development board from NXP.

Sorry, but we do not track all offers from other vendors.

0 件の賞賛
返信