T1024 IFC issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 IFC issue

1,946 Views
sureshk
Contributor II

Hi,

                  In one of our custom board using T1024 Processor received today ,after testing processor has come out of reset and able to connect through JTAG using CW with hardcoded HRCW. and able to access DDR using JTAG intialization file(DDR walk test also passing).

  We tried fusing NOR flash using SRAM file and flash erase itself is failing..After further debugging we found that IFC_CLK itself is not coming from T1024.

  Kindly help us in resolving this issue .

Regards,

   suresh

Labels (1)
Tags (1)
1 Reply

1,750 Views
ufedor
NXP Employee
NXP Employee

Do you see activity of other IFC control signals?

Please note that the IFC clock is active only when there is any access on GPCM or synchronous NOR.