T1024 IFC issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 IFC issue

1,978件の閲覧回数
sureshk
Contributor II

Hi,

                  In one of our custom board using T1024 Processor received today ,after testing processor has come out of reset and able to connect through JTAG using CW with hardcoded HRCW. and able to access DDR using JTAG intialization file(DDR walk test also passing).

  We tried fusing NOR flash using SRAM file and flash erase itself is failing..After further debugging we found that IFC_CLK itself is not coming from T1024.

  Kindly help us in resolving this issue .

Regards,

   suresh

ラベル(1)
タグ(1)
1 返信

1,782件の閲覧回数
ufedor
NXP Employee
NXP Employee

Do you see activity of other IFC control signals?

Please note that the IFC clock is active only when there is any access on GPCM or synchronous NOR.