T1024: How to enable TMU module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024: How to enable TMU module

2,630 Views
gouravjain
Contributor IV

Hi All,
My reference board is based on T1024 reference design. Curently im trying to enable TMU module to measure the temperature of chipset. So far i found thermal driver is required [qoriq_thermal.c].

Would be very thankful if someone help me to know what all things are need to be enabled and how to configure the module ??

Thanks,

Gourav Jain

0 Kudos
Reply
1 Reply

2,626 Views
yipingwang
NXP TechSupport
NXP TechSupport

Kernel configuration:

Platform support --->
      CPU Frequency scaling --->
              PowerPC CPU frequency scaling drivers --->
                        <*> CPU frequency scaling driver for NXP QorIQ SoCs

Device Drivers --->
       [*] Generic Thermal sysfs driver --->
            [*] generic cpu cooling support
            [*] Freescale QorIQ Thermal Monitoring Unit

CONFIG_QORIQ_CPUFREQ=y
CONFIG_THERMAL=y
CONFIG_CPU_THERMAL=y
CONFIG_QORIQ_THERMAL=y

Device Tree Binding

Please add the following in arch/powerpc/boot/dts/fsl/t1024si-post.dtsi, please refer to tmu device node definition in arch/powerpc/boot/dts/fsl/t1023si-post.dtsi.

tmu: tmu@f0000 {
compatible = "fsl,qoriq-tmu", "fsl,t102x-tmu";
reg = <0xf0000 0x1000>;
interrupts = <18 2 0 0>;
fsl,tmu-range = <0xb0000 0xa0026 0x80048 0x30061>;
fsl,tmu-calibration = <0x00000000 0x0000000f

0x00000001 0x00000017
0x00000002 0x0000001e
0x00000003 0x00000026
0x00000004 0x0000002e
0x00000005 0x00000035
0x00000006 0x0000003d
0x00000007 0x00000044
0x00000008 0x0000004c
0x00000009 0x00000053
0x0000000a 0x0000005b
0x0000000b 0x00000064

0x00010000 0x00000011
0x00010001 0x0000001c
0x00010002 0x00000024
0x00010003 0x0000002b
0x00010004 0x00000034
0x00010005 0x00000039
0x00010006 0x00000042
0x00010007 0x0000004c
0x00010008 0x00000051
0x00010009 0x0000005a
0x0001000a 0x00000063

0x00020000 0x00000013
0x00020001 0x00000019
0x00020002 0x00000024
0x00020003 0x0000002c
0x00020004 0x00000035
0x00020005 0x0000003d
0x00020006 0x00000046
0x00020007 0x00000050
0x00020008 0x00000059

0x00030000 0x00000002
0x00030001 0x0000000d
0x00030002 0x00000019
0x00030003 0x00000024>;
little-endian;
#thermal-sensor-cells = <1>;
};

0 Kudos
Reply