T2080 Descriptor Command Fields

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 Descriptor Command Fields

2,051 次查看
chitra_amzarewa
Contributor II

Hello,

I am developing Crypto driver for T2080. Descriptor command fields seem to be confusing.

The macros available in desc.h file of SDK seems to set Command bits following bit positions 31,30,29,28.....2,1,0(MSB-LSB) but for example FIFO LOAD Command Format in the T2080 SEC Reference Manual has the bit positions as 0,1,2.........28,29,30,31(LSB-MSB).

Both fields are contradicting, can you provide additional information if macros in desc.h should be used as is or macros need changes as per T2080SECRM bit ordering?

Any help would be appreciated.

Thanks & Regards,

Chitra Amzarewale

@Faizanbaig 

标签 (1)
0 项奖励
回复
1 回复

2,032 次查看
Faizanbaig
Contributor IV

Could somebody please help us in this?

0 项奖励
回复