T1024-DDR3L Timing Budget Calculator/App Note

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024-DDR3L Timing Budget Calculator/App Note

2,602 Views
mageshmohan
Contributor I

Hi,

I am planning to use the T1024 processor with the DDR3L-On board discrete implementation.

Is there any application notes/tools available for the timing budget calculation.

Regards,

Magesh.M

Labels (1)
0 Kudos
Reply
1 Reply

2,339 Views
r8070z
NXP Employee
NXP Employee


Have a great day

Freescale have provided application note AN3940 “Hardware and Layout Design Considerations for DDR3 SDRAM Memory Interfaces”. There is also Micron’s technical note TN-41-13: “DDR3 Point-to-Point Design Support”.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply