T1024-DDR3L Timing Budget Calculator/App Note

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024-DDR3L Timing Budget Calculator/App Note

2,607件の閲覧回数
mageshmohan
Contributor I

Hi,

I am planning to use the T1024 processor with the DDR3L-On board discrete implementation.

Is there any application notes/tools available for the timing budget calculation.

Regards,

Magesh.M

ラベル(1)
0 件の賞賛
返信
1 返信

2,344件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day

Freescale have provided application note AN3940 “Hardware and Layout Design Considerations for DDR3 SDRAM Memory Interfaces”. There is also Micron’s technical note TN-41-13: “DDR3 Point-to-Point Design Support”.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信