T1024 : BOOT fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 : BOOT fail

1,806 Views
kojimiura
Contributor III

「4.7.1 Power-On Reset Sequence」excerpt 

9. If the IFC's NAND Flash interface is configured as the RCW source, the reset block
instructs the IFC to load a boot block from Flash into the internal buffer RAM of the
IFC. Once complete, the reset block proceeds to instruct the Pre-Boot Loader to
begin reading in RCW data. Note that if the IFC NAND Flash interface reports an
ECC error, the device reset sequence is halted indefinitely, waiting for another
PORESET_B or hard reset.

Is this correct in the interpretation that the CPU stops reading the SPI if there is an error in the RCW (SPI read) data? 

0 Kudos
Reply
2 Replies

1,789 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, correct.

0 Kudos
Reply

1,787 Views
kojimiura
Contributor III

Thank you for answering.

0 Kudos
Reply