T1024 : BOOT fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 : BOOT fail

1,823件の閲覧回数
kojimiura
Contributor III

「4.7.1 Power-On Reset Sequence」excerpt 

9. If the IFC's NAND Flash interface is configured as the RCW source, the reset block
instructs the IFC to load a boot block from Flash into the internal buffer RAM of the
IFC. Once complete, the reset block proceeds to instruct the Pre-Boot Loader to
begin reading in RCW data. Note that if the IFC NAND Flash interface reports an
ECC error, the device reset sequence is halted indefinitely, waiting for another
PORESET_B or hard reset.

Is this correct in the interpretation that the CPU stops reading the SPI if there is an error in the RCW (SPI read) data? 

0 件の賞賛
返信
2 返答(返信)

1,806件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes, correct.

0 件の賞賛
返信

1,804件の閲覧回数
kojimiura
Contributor III

Thank you for answering.

0 件の賞賛
返信