T1024 Aurora interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 Aurora interface

2,033 Views
safeerkt
Contributor II

Hi,

We are in the design face of T1024 based board.We would like to add Aurora debug interface in the board.

Is there any documents available which can help us regarding the pin mapping,aurora debug connector pin out etc..?

Also please share the link if you have any reference schematics which can help us for the same..

Many Thanks,

Safeer.

Labels (1)
0 Kudos
Reply
1 Reply

1,786 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1024QDS support Aurora debug with dedicated connectors. I suggest you to create a Technical case with request for the T1024QDS schematics sheets realted to the Aurora debug port. Please see
How I could create a Technical Case?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply