T1022 Processor configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1022 Processor configuration

1,746 次查看
swatig
Contributor I

Hello All,

I am using T1022 processor in one of the designs. In the design, I do not want to use the RGMII/MII on EC1 or EC2 interface, but want to use only MDIO at 2.5V. I understand that for this use case:
-> power L1VDD and LVDD will have to be kept at 2.5V
-> EC1 and EC2 will be configured as GPIOs and 
-> there will be no requirement for oscillator on EC*_GTX_CLK125.

Can someone confirm whether it is a valid configuration or not?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,729 次查看
r8070z
NXP Employee
NXP Employee

It is a valid configuration.