T1022 IFC LSB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1022 IFC LSB

2,495 Views
jack_mcculloch
Contributor I

Hi,

We would like to connect a TL16C752D Dual UART to the IFC bus on the T1022. We are assuming the GPCM mode is the most suitable for this application?

We are also unsure what LSB of address and data bus should be?

Should the address start at IFC_A31?

Is the Data bus LSB IFC_AD7 and MSB IFC_AD0?

Labels (1)
0 Kudos
Reply
3 Replies

2,470 Views
jack_mcculloch
Contributor I

Thanks.

And how do we align the data bus if we are using 8 bits?

0 Kudos
Reply

2,464 Views
r8070z
NXP Employee
NXP Employee

Connect 8-bit port  to AD[0:7], AD0 is the most significant bit.

 

0 Kudos
Reply

2,479 Views
r8070z
NXP Employee
NXP Employee

In the normal GPCM mode of operation ADDR bus carries the least significant bits. ADDR[31] will carry the lsb of the system address.

0 Kudos
Reply