T1022 IFC LSB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1022 IFC LSB

2,499 次查看
jack_mcculloch
Contributor I

Hi,

We would like to connect a TL16C752D Dual UART to the IFC bus on the T1022. We are assuming the GPCM mode is the most suitable for this application?

We are also unsure what LSB of address and data bus should be?

Should the address start at IFC_A31?

Is the Data bus LSB IFC_AD7 and MSB IFC_AD0?

标签 (1)
0 项奖励
回复
3 回复数

2,474 次查看
jack_mcculloch
Contributor I

Thanks.

And how do we align the data bus if we are using 8 bits?

0 项奖励
回复

2,468 次查看
r8070z
NXP Employee
NXP Employee

Connect 8-bit port  to AD[0:7], AD0 is the most significant bit.

 

0 项奖励
回复

2,483 次查看
r8070z
NXP Employee
NXP Employee

In the normal GPCM mode of operation ADDR bus carries the least significant bits. ADDR[31] will carry the lsb of the system address.

0 项奖励
回复