T1022 Example Secureboot RCW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1022 Example Secureboot RCW

4,160 Views
tschutte
Contributor III


Looking for an example RCW that someone has used to successfully boot SecureBoot on a T1022. I have one that I think should be working (Modified memory map, scratch registers being set, etc) but when I change the SB_EN bit = 1 I hit a machine check.

Labels (1)
0 Kudos
Reply
5 Replies

3,845 Views
bpe
NXP Employee
NXP Employee

T1022 is a proper subset of T1042. QorIQ SDK includes ready and verified secure boot RCWs  for T1042RDB and T1042RDB-PI. Unpack the package called 'rcw', inspect the source. Detailed instructions can be found here:

Submit Form

Submit Form


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,845 Views
tschutte
Contributor III

I'm not seeing a 'rcw' package anywhere in the SDK. Where can I download the package from?

0 Kudos
Reply

3,845 Views
bpe
NXP Employee
NXP Employee

You do not have to download anything in addition to the SDK source DVD image. rcw package is part of the SDK:

$ bitbake -s | grep rcw

rcw                                                   :git-r0                         

Install the SDK and follow instructions at the links I posted above to unpack the package and inspect it's source.


Have a great day,

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,845 Views
tschutte
Contributor III

So I got RCW's but didnt see any for the T1042, are they not part of the 2.0 SDK?

0 Kudos
Reply

3,845 Views
tschutte
Contributor III

Is there a way to get the RCW's without downloading the full SDK? Or could someone Just post the contents of the RCW?

0 Kudos
Reply