T1022 Clock Sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1022 Clock Sequence

Jump to solution
1,703 Views
jack_mcculloch
Contributor I

Hi,

 

We are designing a custom board with a T1022 processor and would like to know if the there are any power-on sequencing requirements for the clocks?

 

Do all power rails need to be valid before clocks are enabled?

 

Is there minimum time the clocks need to be valid before PORESET_B is lifted?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,588 Views
Bulat
NXP Employee
NXP Employee

SYSCLK can be applied alone with OVDD/O1VDD supplies.
We do not specify "minimum time the clocks need to be valid before PORESET_B".
Minimum PORESET assertion time is 1ms, use it as a 'clock valid' setup as well.

Regards,

Bulat

View solution in original post

0 Kudos
Reply
1 Reply
1,589 Views
Bulat
NXP Employee
NXP Employee

SYSCLK can be applied alone with OVDD/O1VDD supplies.
We do not specify "minimum time the clocks need to be valid before PORESET_B".
Minimum PORESET assertion time is 1ms, use it as a 'clock valid' setup as well.

Regards,

Bulat

0 Kudos
Reply