T1022 Clock Sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,692件の閲覧回数
jack_mcculloch
Contributor I

Hi,

 

We are designing a custom board with a T1022 processor and would like to know if the there are any power-on sequencing requirements for the clocks?

 

Do all power rails need to be valid before clocks are enabled?

 

Is there minimum time the clocks need to be valid before PORESET_B is lifted?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,577件の閲覧回数
Bulat
NXP Employee
NXP Employee

SYSCLK can be applied alone with OVDD/O1VDD supplies.
We do not specify "minimum time the clocks need to be valid before PORESET_B".
Minimum PORESET assertion time is 1ms, use it as a 'clock valid' setup as well.

Regards,

Bulat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,578件の閲覧回数
Bulat
NXP Employee
NXP Employee

SYSCLK can be applied alone with OVDD/O1VDD supplies.
We do not specify "minimum time the clocks need to be valid before PORESET_B".
Minimum PORESET assertion time is 1ms, use it as a 'clock valid' setup as well.

Regards,

Bulat

0 件の賞賛
返信