Support for DPAA1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for DPAA1

Jump to solution
2,378 Views
ramkrishnan
Contributor III

This is a question regarding DPAA1 and DPAA2. If I am to decide on a chipset primarily used for network packet processing, is it better to wait for a chipset that supports DPAA2 or go with the T4240 which supports DPAA1. Will the DPAA1 go away and be replaced with DPAA2. It is also nice that the DPAA2 has the ODP support. I also see that some demo applications that were supported on the older SDK's are not there anymore on the newer 1.9 and 2.0 SDK's. Any recommendations will be helpful..

Regards,

Ram

0 Kudos
Reply
1 Solution
2,000 Views
bpe
NXP Employee
NXP Employee

If you wish to start your design now, and you need the maximum performance

device, then select T4240. It's part of the longevity program, if that

is your concern:

http://www.nxp.com/about/technology-leadership/product-longevity/product-longevity-nxp-formerly-free...

DPAA2-based devices of a comparable packet processing performance are

future products,  their schedule is NDA information. If you are

interested in future chips, discuss it with your distributor.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,001 Views
bpe
NXP Employee
NXP Employee

If you wish to start your design now, and you need the maximum performance

device, then select T4240. It's part of the longevity program, if that

is your concern:

http://www.nxp.com/about/technology-leadership/product-longevity/product-longevity-nxp-formerly-free...

DPAA2-based devices of a comparable packet processing performance are

future products,  their schedule is NDA information. If you are

interested in future chips, discuss it with your distributor.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply