SDK SRA source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,946件の閲覧回数
tapyang
Contributor III

Dear, All:

I am developing the SRIO application of T2080, so I wanna refer to the SRA application code.

And I can not find it in SDK, where can I find it?

ps:My SDK is "QorIQ Linux SDK v2.0 SOURCE", and it says:

"10.7.16.1.2.2 SDK Installation
SRA is based on NXP Linux SDK. So to use SRA, make sure NXP Linux SDK is well installed."

Looking forward to your reply and thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,819件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Chapter 9.9.16 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,820件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Chapter 9.9.16 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信