SDK SRA source code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDK SRA source code

跳至解决方案
1,961 次查看
tapyang
Contributor III

Dear, All:

I am developing the SRIO application of T2080, so I wanna refer to the SRA application code.

And I can not find it in SDK, where can I find it?

ps:My SDK is "QorIQ Linux SDK v2.0 SOURCE", and it says:

"10.7.16.1.2.2 SDK Installation
SRA is based on NXP Linux SDK. So to use SRA, make sure NXP Linux SDK is well installed."

Looking forward to your reply and thanks!

标签 (1)
0 项奖励
回复
1 解答
1,834 次查看
Pavel
NXP Employee
NXP Employee

Look at the Chapter 9.9.16 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,835 次查看
Pavel
NXP Employee
NXP Employee

Look at the Chapter 9.9.16 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复