Regarding SSD interfacing with T1042

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding SSD interfacing with T1042

4,167 Views
sarkarsouvik
Contributor II

Hello All,

In one of our current prototype designs, we wanted to interface an SSD with the T1042 processor. Normally we would use SATA as the interface. My question is weather we can use PCIe x2 lane from the 85h configuration to mount an NVMe SSD. 

Also, does T1042 support M.2 SSDs on either SATA or PCIe?

Thank you. Your help in this case is greatly appreciated.

Regards,

Souvik

Labels (1)
0 Kudos
Reply
6 Replies

4,146 Views
sarkarsouvik
Contributor II

Please help in this regard. It is urgently required. Thank you.

0 Kudos
Reply

4,136 Views
Pavel
NXP Employee
NXP Employee

Look at the following page about similar problem:

https://blog.csdn.net/Zhu_Zhu_2009/article/details/89084729

 

Try to test your board using SDK 2.7:

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/about/

0 Kudos
Reply

4,130 Views
sarkarsouvik
Contributor II

Hello Pavel,

Thank you for your reply. However, my question is whether M.2 form factor SSD is supported with the SATA interface present in 86h configuration of T1042.

Also, as an alternate in 85h configuration of T1042, whether M.2 NVMe SSD is supported in the PCIe x2 lanes of the processor.

Thanks.

0 Kudos
Reply

4,124 Views
Pavel
NXP Employee
NXP Employee

The T1042 supports SATA if the SRDS_PRTCL_S1 is set to 0x86.

See the Figure 31-1 in the T1042 Reference Manual:

https://www.nxp.com/webapp/Download?colCode=T1040RM

4,121 Views
sarkarsouvik
Contributor II

Thank you for your confirmation. 

Can you also let us know whether we can use an SSD with the PCIe x2 lane present in 85h configuration?

0 Kudos
Reply

4,114 Views
Pavel
NXP Employee
NXP Employee

The T1042 SerDes does not support SATA if the SRDS_PRTCL_S1 is set to 0x85.

See the Figure 31-1 in the T1042 Reference Manual:

https://www.nxp.com/webapp/Download?colCode=T1040RM

0 Kudos
Reply