Regarding SSD interfacing with T1042

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding SSD interfacing with T1042

4,187件の閲覧回数
sarkarsouvik
Contributor II

Hello All,

In one of our current prototype designs, we wanted to interface an SSD with the T1042 processor. Normally we would use SATA as the interface. My question is weather we can use PCIe x2 lane from the 85h configuration to mount an NVMe SSD. 

Also, does T1042 support M.2 SSDs on either SATA or PCIe?

Thank you. Your help in this case is greatly appreciated.

Regards,

Souvik

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

4,166件の閲覧回数
sarkarsouvik
Contributor II

Please help in this regard. It is urgently required. Thank you.

0 件の賞賛
返信

4,156件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following page about similar problem:

https://blog.csdn.net/Zhu_Zhu_2009/article/details/89084729

 

Try to test your board using SDK 2.7:

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/about/

0 件の賞賛
返信

4,150件の閲覧回数
sarkarsouvik
Contributor II

Hello Pavel,

Thank you for your reply. However, my question is whether M.2 form factor SSD is supported with the SATA interface present in 86h configuration of T1042.

Also, as an alternate in 85h configuration of T1042, whether M.2 NVMe SSD is supported in the PCIe x2 lanes of the processor.

Thanks.

0 件の賞賛
返信

4,144件の閲覧回数
Pavel
NXP Employee
NXP Employee

The T1042 supports SATA if the SRDS_PRTCL_S1 is set to 0x86.

See the Figure 31-1 in the T1042 Reference Manual:

https://www.nxp.com/webapp/Download?colCode=T1040RM

4,141件の閲覧回数
sarkarsouvik
Contributor II

Thank you for your confirmation. 

Can you also let us know whether we can use an SSD with the PCIe x2 lane present in 85h configuration?

0 件の賞賛
返信

4,134件の閲覧回数
Pavel
NXP Employee
NXP Employee

The T1042 SerDes does not support SATA if the SRDS_PRTCL_S1 is set to 0x85.

See the Figure 31-1 in the T1042 Reference Manual:

https://www.nxp.com/webapp/Download?colCode=T1040RM

0 件の賞賛
返信