QCVS error configuring NOR FLASH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QCVS error configuring NOR FLASH

8,882件の閲覧回数
sergiohernandez
Contributor I

I'm generatin a new RCW with QCVS 4.5 for a T2080 board.

When I try to configure RCW_SRC, PBI_SRC and BOOT_LOC to NOR Flash, QCVS shows an error, why?

pastedImage_0.png

When I change PBI_SRC or BOOT_LOC to another interface there is no error.

If I try the same configuration with previous versions of QVCS (4.2.1) there is no error for this configuration.

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

8,507件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please upgrade to QCVS 4.5 which is the latest release.

Adrian

0 件の賞賛
返信

8,507件の閲覧回数
sergiohernandez
Contributor I

Ok, after update no error is show.

Thank you.

De: addiyi

Enviado el: lunes, 30 de mayo de 2016 13:23

Para: Hernández Sánchez, Sergio

Asunto: Re: - QCVS error configuring NOR FLASH

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

QCVS error configuring NOR FLASH

reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655533?et=watches.email.thread#comment-655533>

0 件の賞賛
返信

8,507件の閲覧回数
addiyi
NXP Employee
NXP Employee

It is just an warning. You can ignore it by selecting Advanced tab and Ignore Constrains and Non-Critical errors.

pastedImage_0.png

Adrian

0 件の賞賛
返信

8,507件の閲覧回数
sergiohernandez
Contributor I

Ok, but why it is considered an ERROR, I think it is a valid configuration.

De: addiyi

Enviado el: lunes, 30 de mayo de 2016 9:38

Para: Hernández Sánchez, Sergio

Asunto: Re: - QCVS error configuring NOR FLASH

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

QCVS error configuring NOR FLASH

reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655446?et=watches.email.thread#comment-655446>

0 件の賞賛
返信

8,507件の閲覧回数
addiyi
NXP Employee
NXP Employee

Could you add your PBL binary? Also, what Soc rev have you selected?

Adrian

0 件の賞賛
返信

8,504件の閲覧回数
sergiohernandez
Contributor I

I’ve selected V1.1

PBL generated is attached to this email.

De: addiyi

Enviado el: lunes, 30 de mayo de 2016 10:15

Para: Hernández Sánchez, Sergio

Asunto: Re: - QCVS error configuring NOR FLASH

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

QCVS error configuring NOR FLASH

reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655496?et=watches.email.thread#comment-655496>

0 件の賞賛
返信

8,504件の閲覧回数
addiyi
NXP Employee
NXP Employee

No error on my side:

pastedImage_0.png

Could you please provide the QCVS build number. Go to Help > About CodeWarrior, click on QCVS icon and provide the version number.

Adrian

0 件の賞賛
返信

8,504件の閲覧回数
sergiohernandez
Contributor I

I’m using eclipse version installed in VirtualBox provided by NXP witk SDK 1.9

De: addiyi

Enviado el: lunes, 30 de mayo de 2016 12:56

Para: Hernández Sánchez, Sergio

Asunto: Re: - QCVS error configuring NOR FLASH

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

QCVS error configuring NOR FLASH

reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655531?et=watches.email.thread#comment-655531>

0 件の賞賛
返信