Probability for CPU producing identical data in lockstep architecture?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Probability for CPU producing identical data in lockstep architecture?

489件の閲覧回数
Xingzi
Contributor I

If there is lockstep design to monitor the CPU T2081 output, what is the probability defeating the lockstep mechanism such as producing the identical erroneous data?

For example, if the data size of CPU output is 64 bits, could the probability of 2 CPUs producing the same erroneous data is 1/64*P(CPU0 Error)*P(CPU1 Error)?

The factor 1/data length could be used? Or what is the factor if not?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

472件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

There are no hardware provisions for that in any T-series or P-series processor and no recommendations for implementing it are available.

0 件の賞賛
返信