Packets generator with DPAA ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Packets generator with DPAA ?

ソリューションへジャンプ
3,200件の閲覧回数
nicolaskury
Contributor II

Hi

I would like to compare the network throughtput when I send packets using Linux sockets versus when I send with DPAA.

Does a packets generator using DPAA already exist ? Where can I find it ?

Thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
3,022件の閲覧回数
bpe
NXP Employee
NXP Employee

There is a little confusion. Linux kernel network interface driver for DPAA-enabled chips

utilizes all three main components of DPAA, FMAN, BMAN and QMAN, to process your data.

There is no way to bypass DPAA.

If you meant USDPAA, which is a software that allows userspace tasks to enqueue/deque

network packets directly to/from QMAN, it does not have any ready traffic generator.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,023件の閲覧回数
bpe
NXP Employee
NXP Employee

There is a little confusion. Linux kernel network interface driver for DPAA-enabled chips

utilizes all three main components of DPAA, FMAN, BMAN and QMAN, to process your data.

There is no way to bypass DPAA.

If you meant USDPAA, which is a software that allows userspace tasks to enqueue/deque

network packets directly to/from QMAN, it does not have any ready traffic generator.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,022件の閲覧回数
nicolaskury
Contributor II

Thank you!

0 件の賞賛
返信