PTP/IEEE 1588 on multiple frame managers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTP/IEEE 1588 on multiple frame managers

1,635 Views
björnolofsson
Contributor I

The manual for the IEEE 1588 Device Driver states under Known bugs and limitations that "For DPAA, the PTPd stack limits to use only one ptp timer, so only the interfaces on the second FMAN(such as fm2-gb2) are available for PTPd if the platform has two FMANs" Is this a hardware limitation or just a limitation for the device driver?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,363 Views
Pavel
NXP Employee
NXP Employee

It is driver limitation. The QorIQ errata list does not have information about similar limitation. The IEEE 1588-2008 Quick Start was developed for the P1025-TWR board. There is no the second FMAN on the P1025.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply