PCIe in End Point mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe in End Point mode

4,379 Views
leventkarakaya
Contributor I

Hello,

I am trying to use QorIQ T1024 processor's PCIe port in End Point mode. My aim is to configure T1024 behave as a Memory Controller device on pci bus.

From reference manual, I understood that I need to set the pcie port to End Point mode in RCW to configure hardware. What else should I do to configure Software side? I need Bars and set MSI interrupts to communicate with Host. Is it the same way as in RC mode? Can anybody share a sample code?

Best regards

Labels (1)
0 Kudos
Reply
1 Reply

3,524 Views
ufedor
NXP Employee
NXP Employee

Please refer to the attached document.

0 Kudos
Reply