as given in the board we have 8 ethernet ports so how we can use that ports ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

as given in the board we have 8 ethernet ports so how we can use that ports ?

1,371件の閲覧回数
loliyana_jay199
Contributor II

like we want to use eth-3 or eth-4 ports in our application for transmit and receive data so how we can use that ports ?

is there any reference manual for that ? 

and my second doubt is that how we can use DPAA for that ports ?

ラベル(1)
タグ(3)
2 返答(返信)

1,221件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello jay loliyana,

What target board or processor are you using?

Did you developed Linux application or bareboard application? If so, your could refer to busy box ping application.

DPAA (Data Path Acceleration Architecture) hardware inspects ingress traffic and extracts user defined flows from the port traffic. It then steers specific flows (or related traffic) to a specific core or set of cores.

DPAA driver is enabled in Linux Kernel by default.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,221件の閲覧回数
loliyana_jay199
Contributor II

i m using bare-board application sir .

as you said that by busy box ping application what is that ?

how can i find that application n how we can use that ethernet port .

0 件の賞賛
返信