Missing base address of CPC Partitioning Control Registers in user documentation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Missing base address of CPC Partitioning Control Registers in user documentation

跳至解决方案
2,333 次查看
nakrachi
Contributor II

Hi Everyone,

As part of the platform cache flushing procedure, the T1042 RM states that "Clear all bits in CPCPAR0-CPCPAR15 " but we couldn;t find the base address of CPCPAR in the reference manual.

nakrachi_2-1634136827775.png

it looks like it was removed :

nakrachi_0-1634136492182.png

I know (using the Trace32) that the base address for CPC_PAR0 is CROSSBAR_ADR+0x10208, but we need to confirm this with NXP to document it as a rational.

thank you

0 项奖励
回复
1 解答
2,328 次查看
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

CPC_CPCPAR0 address is equal to:

base address (specified by the CCSRBAR) + 0x1_0000 (CPC block offset address) + 0x208

在原帖中查看解决方案

2 回复数
2,329 次查看
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

CPC_CPCPAR0 address is equal to:

base address (specified by the CCSRBAR) + 0x1_0000 (CPC block offset address) + 0x208

2,322 次查看
nakrachi
Contributor II

Thank you

标记 (1)
0 项奖励
回复