Missing base address of CPC Partitioning Control Registers in user documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing base address of CPC Partitioning Control Registers in user documentation

Jump to solution
2,427 Views
nakrachi
Contributor II

Hi Everyone,

As part of the platform cache flushing procedure, the T1042 RM states that "Clear all bits in CPCPAR0-CPCPAR15 " but we couldn;t find the base address of CPCPAR in the reference manual.

nakrachi_2-1634136827775.png

it looks like it was removed :

nakrachi_0-1634136492182.png

I know (using the Trace32) that the base address for CPC_PAR0 is CROSSBAR_ADR+0x10208, but we need to confirm this with NXP to document it as a rational.

thank you

0 Kudos
Reply
1 Solution
2,422 Views
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

CPC_CPCPAR0 address is equal to:

base address (specified by the CCSRBAR) + 0x1_0000 (CPC block offset address) + 0x208

View solution in original post

2 Replies
2,423 Views
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

CPC_CPCPAR0 address is equal to:

base address (specified by the CCSRBAR) + 0x1_0000 (CPC block offset address) + 0x208

2,416 Views
nakrachi
Contributor II

Thank you

Tags (1)
0 Kudos
Reply