MDIO connection for SGMII interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MDIO connection for SGMII interface

1,743 次查看
ajaykumardangi
Contributor I


Hi

I am using T1024 and have connected 3 1G ethernet to it. out of 3 1G ethernet one is RGMII and its MDIO is connected to MDIO1, other 2 ethernet are SGMII and conned to lane 1 and lane 2. The MDIO signal related to lane 1 and 2 (SGMII) should be conned to MDIO1 or MDIO2?

标签 (1)
0 项奖励
回复
1 回复

1,482 次查看
alexander_yakov
NXP Employee
NXP Employee

MDIO2 interface output buffers are powered from 1.2V voltage rail (TVDD), this interface is intended to be used for low voltage MDIO connections, typically - to manage 10G PHYs.

0 项奖励
回复