At present, there is sdk 1.9 release is out but it is also with kernel version 3.12. For our product we need some features which requires at-least kernel version 3.14 or higher. So, would like to know that is there any plan on releasing SDK 2.0 and if yes, what is the kernel version it will based on?
Also, is there anyways I can have hands on the beta release or pre-release of it ?
SDKs are released twice a year. The upcoming SDK 2.0 will be based on Kernel 4.1.8, planned to be released in May.
For any pre-release version access, approach your FAE or distributor:
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------