L2 cache coherence issue on e6500 Rev-2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

L2 cache coherence issue on e6500 Rev-2.0

910 次查看
yintai_shao
Contributor I

There is an e6500 L2 cache issue perplexed me.

Target board:   T4240QDS and T2080QDS

Core version:   e6500 REV-2.0

OS:                     WindRiver's VxWorks SMP system

Boot loader:     u-boot

Phenomenon description:

In my test case, one of the T4240 (or T2080) core continues to write an increased value to a specified memory address (this space is pointed by pMemAddr). The address is could be accessed for other cores. The operation just likes,

         *(volatile UINT32 *)(pMemAddr) = 0;

         while (testRun)

            {

            (*(volatile unsigned int *)(pMemAddr))++;

            }

This core, I name it as writer in here.

Another core continues to check whether the context in the memory address is changed or not. I named this core as reader. The reader just could find the context in the memory (pointed by pMemAddr) is changed from the initialized value (deadbeef) to 0 and kept, no more changed again.

If the write instruction in the loop is followed by a memory barrier instruction, then the reader could find the memory context is changed in real time, the coherence issue will be no more.

         *(volatile UINT32 *)(pMemAddr) = 0;

         while (testRun)

            {

            (*(volatile unsigned int *)(pMemAddr))++;

            __asm volatile(" sync ");

            }

This issue is occurred only on CPU with e6500 REV-2.0 core, such as T4240 REV-2.0 and T2080 REV-1.0, but not on T4240 REV-1.0 (e6500 REV-1.0), e5500 core types (T1040E) and e500mc types (P4080E).

Why this issue occurred?

What is difference between e6500 REV-1.0 and REV-2.0?

Whether is the memory barrier instruction is needed on this condition the in normal?

Thanks

Yintai Shao

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数