Is secure boot possible only via NOR boot in T1024 processor?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is secure boot possible only via NOR boot in T1024 processor?

跳至解决方案
3,091 次查看
arumugamp
Contributor I

From QorIQ SDKv2.0 documentation, for T1 series it is mentioned only via NOR, secure boot is possible.  Please get this clear to me.  Thanks in advance.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,948 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello ARUMUGAM P,

On T1024, secure boot could be implemented from NAND.

But in SDK 2.0, no software support for T1024 NAND secure boot.

You could modify RCW(PBI support) and u-boot source code by yourself, you could refer to P3041DS.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,948 次查看
Pavel
NXP Employee
NXP Employee

NXP SDK 2.0 supports secure boot for the T1024RDB board. See attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,948 次查看
arumugamp
Contributor I

Thanks Pavel.  But whether the secure boot could be implemented from NAND in T1024?

0 项奖励
回复
2,949 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello ARUMUGAM P,

On T1024, secure boot could be implemented from NAND.

But in SDK 2.0, no software support for T1024 NAND secure boot.

You could modify RCW(PBI support) and u-boot source code by yourself, you could refer to P3041DS.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复