Is secure boot possible only via NOR boot in T1024 processor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is secure boot possible only via NOR boot in T1024 processor?

Jump to solution
3,074 Views
arumugamp
Contributor I

From QorIQ SDKv2.0 documentation, for T1 series it is mentioned only via NOR, secure boot is possible.  Please get this clear to me.  Thanks in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,931 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello ARUMUGAM P,

On T1024, secure boot could be implemented from NAND.

But in SDK 2.0, no software support for T1024 NAND secure boot.

You could modify RCW(PBI support) and u-boot source code by yourself, you could refer to P3041DS.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,931 Views
Pavel
NXP Employee
NXP Employee

NXP SDK 2.0 supports secure boot for the T1024RDB board. See attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,931 Views
arumugamp
Contributor I

Thanks Pavel.  But whether the secure boot could be implemented from NAND in T1024?

0 Kudos
Reply
2,932 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello ARUMUGAM P,

On T1024, secure boot could be implemented from NAND.

But in SDK 2.0, no software support for T1024 NAND secure boot.

You could modify RCW(PBI support) and u-boot source code by yourself, you could refer to P3041DS.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply