Is SPL image support NOR flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is SPL image support NOR flash?

ソリューションへジャンプ
3,117件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All.

I am working on T4160RDB. I built u-boot-spl.bin and flash using NOR. But, I have a doubt, is it SPL really work in NOR?

or is SPL image suitable for NAND and SDcard?

Regards,

VinothS

Regards,
Vinothkumar Sekar
ラベル(3)
0 件の賞賛
返信
1 解決策
2,881件の閲覧回数
ufedor
NXP Employee
NXP Employee

SPL executed from SRAM is required for SD and NAND boot because direct code execution from these devices is not possible - it is required to read block of data to SRAM and execute it from there.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,882件の閲覧回数
ufedor
NXP Employee
NXP Employee

SPL executed from SRAM is required for SD and NAND boot because direct code execution from these devices is not possible - it is required to read block of data to SRAM and execute it from there.

0 件の賞賛
返信
2,881件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply.

So, there is no possible to use SPL binary for NOR flash.

Is it right ?

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
2,881件の閲覧回数
ufedor
NXP Employee
NXP Employee

Yes.

0 件の賞賛
返信
2,881件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you

Regards,
Vinothkumar Sekar
0 件の賞賛
返信