Is SPL image support NOR flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is SPL image support NOR flash?

Jump to solution
3,127 Views
vinothkumars
Senior Contributor IV

Hi All.

I am working on T4160RDB. I built u-boot-spl.bin and flash using NOR. But, I have a doubt, is it SPL really work in NOR?

or is SPL image suitable for NAND and SDcard?

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1 Solution
2,891 Views
ufedor
NXP Employee
NXP Employee

SPL executed from SRAM is required for SD and NAND boot because direct code execution from these devices is not possible - it is required to read block of data to SRAM and execute it from there.

View solution in original post

0 Kudos
Reply
4 Replies
2,892 Views
ufedor
NXP Employee
NXP Employee

SPL executed from SRAM is required for SD and NAND boot because direct code execution from these devices is not possible - it is required to read block of data to SRAM and execute it from there.

0 Kudos
Reply
2,891 Views
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply.

So, there is no possible to use SPL binary for NOR flash.

Is it right ?

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply
2,891 Views
ufedor
NXP Employee
NXP Employee

Yes.

0 Kudos
Reply
2,891 Views
vinothkumars
Senior Contributor IV

Thank you

Regards,
Vinothkumar Sekar
0 Kudos
Reply