The original question was support for the T1040D4RDB-PB in SDK 2.0.
The table in the document indicates that the PB version of the T1040D4RDB is only supported in SDK 1.6 and 1.7.
T1040/ T1020 N N N N N rev 1.0 rev 1.1 rev 1.1 rev 1.1 rev 1.1 rev 1.1 rev 1.1 rev 1.1
T1040RDBPB N N N N N ✔ ✔ N N N N N N
T1040D4RD B-PA N N N N N N N ✔ ✔ ✔ ✔ ✔ ✔
I need to be able to access the L2 switch settings which I believe was added in SDK 1.8 and above.
So I guess the question becomes what is different between the PA and PB versions of the T1040D4RDB hardware that prevents the PB version from being supported in SDK 2.0?
Or to put it another way, what needs to be done to get SDK 2.0 running on the PB version of the T1040D4RDB?